FLIR Introduces Raymarine Axiom XL Multifunction Displays For Premium Yachts and Glass Bridge Installs

/globalassets/news/1200x628_axiomxl.jpg

Today, FLIR announced the introduction Raymarine®’s flagship line of multifunction displays (MFDs), Axiom™ XL. Designed for premium yachts and glass bridge installations, Axiom XL displays offer the largest size in the Axiom family and the superior performance and elegant simplicity that the award-winning Axiom line has delivered since its introduction.

Engineered to perform in extreme marine conditions, the Axiom XL family is fully waterproof and can be installed in both open cockpits and enclosed bridge stations. Each model uses in-plane switching (IPS) and Raymarine’s optical bonding display technology to deliver wider viewing angles, sharp contrast, and unmatched readability in bright sun. Available in 16-, 19-, 22- and 24-inch display sizes, Axiom XL’s edge-to-edge glass construction gives vessel designers the ability to create a seamless navigation helm.

Axiom XL is a powerful network and video integration platform featuring three Ethernet ports for connecting with network sensors or with additional Axiom, Axiom Pro, and Axiom XL family displays. This simplified integration allows boat designers greater flexibility when creating multi-display and multi-station navigation systems. Axiom XL’s native FLIR thermal imaging camera support enhances navigation awareness and safety, while HDMI input enables Axiom XL to serve as a remote touchscreen PC or entertainment display at the helm. 

At the heart of each Axiom XL display is a fast quad core processor that supports Raymarine navigation, radar, sonar, and FLIR thermal technology for an all-in-one, full-high-definition (HD) display solution. Powered by Raymarine’s LightHouse 3 Operating System, Axiom XL displays offer an elegant, intuitive, uncluttered interface that is fast, fluid, and easily personalized for each captain’s navigation style. Captains have the choice of multi-touch screen control or the Raymarine RMK-10 keypad for complete remote system control of multiple Axiom XL displays.

The Axiom XL16 and X19 displays are available NOW through FLIR’s network of marine electronics dealers. The Axiom XL24 will be available in July, followed by Axiom XL22 in September. Pricing for Axiom XL MFDs starts at $6,799.99 USD.

For more information on the Raymarine Axiom XL visit Raymarine.com/AxiomXL.

 

Related Articles