Introducing FLIR Saros Dome Outdoor Perimeter Security Cameras

/globalassets/news/1200x628_saros_product-image_right-copy.jpg

Today at the 2018 IFSEC International Tradeshow in London, FLIR introduced the first product family of the new Saros outdoor perimeter security cameras, the FLIR Saros Dome cameras. The Saros dome family combines patented and patent pending technologies in a unified solution for accurate alerts and verified alarm data for outdoor commercial perimeters.

The FLIR Saros Dome integrates multiple technologies in one device, including two low-cost FLIR Lepton® thermal sensors supported by advanced onboard analytics, IR and visible LED illuminators, 2-way audio and digital input/outputs, and the choice of a 1080p or 4K video camera. The FLIR Saros Dome camera line allows more business owners to benefit from the detection advantages of thermal imaging for perimeter and wide area protection. FLIR Saros Dome not only reduces the cost of initial deployment by minimizing equipment requirements, but also reduces false alarms with built-in advanced analytics. Integration with central alarm monitoring stations will expand the outdoor perimeter protection opportunities for security dealers.

FLIR Saros Dome models will begin shipping in North America and Europe in the third quarter of 2018 through FLIR’s established network of dealers and integrators.

  • FLIR Saros DH-390 2MP (1080p camera)and FLIR Saros DH-390 8MP (4K camera) offer a thermal resolution of 320x120 with a 90-degree field-of-view.

For more information on FLIR Saros Dome, visit FLIR.com/Saros (United States) and FLIR.eu/Saros (Europe).

Related Articles