Icon-ContactSales Grid View Exported from Streamline App (https://app.streamlineicons.com) Model Selector Model Selector
You must be logged in to download this content. Please sign in or create an account here.
What is the typical spectral response for certain camera/lens combination?
This curve is valid for the following lenses:
IR lens, f=88.9 mm (7°)
IR lens, f=41.3 mm (15°)
IR lens, f=24.6 mm (25°)
IR lens, f=13.1 mm (45°)
This curve is valid for the following lenses:
IR lens, f=6.5 mm (80°)
Close-up IR lens, 2.9× (50 µm)
Close-up IR lens, 5.8× (100 µm)
This curve is valid for the following lens:
Close-up IR lens, 1.5× (25 µm)
Trouble Shooting
My measurement tools are changing location when I open the image in edit mode compared with the overview mode? Why is that?
Read the Story
Technical Guidance
What are the key features of ThermaCAM™ P50F and P25F?
Read the Story
Trouble Shooting
Why is there a charging animation on the screen of the camera, despite the fact that the battery was charged for a whole night in the in-truck charger?
Read the Story