Support Center

Bench Instruments - Decade Boxes

All Products (2) Grid view Grid view List View List View

Extech 380400

The Extech 380400 Resistance Decade Box is very popular for product design testing and calibration because it can be substituted into a circuit and function in the place of any component with a standard value easily. Alternatively, it can be used to identify the best value for circuit operation then read that value from the switches. Then, a resistor of the size indicated by the decade box switches can be put into the circuit.

Extech 380405

The Extech 380405 Capacitance Decade Box is very popular for product design testing and calibration because it can be substituted into a circuit and function in the place of any component with a standard value easily. Alternatively, it can be used to identify the best value for circuit operation, then read that value from the switches. A capacitor of the size indicated by the decade box switches can then be put into the circuit.